Skip to main content
elv.1
Associate
Oct 17, 2022 7:30 AM UTC
Question

Can I configure to broadcast multiple different frames?

  • I tried broadcasting 6 different frames of data,Is that possible?Here is my configuration.thanks my brother.

​

uint8_t adv_bag1[] = {0x02,0x01,0x06,0x10,0x09,'M','i','n','e','w','-','B','L','E','-','T','e','s','t','1'};
uint8_t adv_bag2[] = {0x02,0x01,0x06,0x10,0x09,'M','i','n','e','w','-','B','L','E','-','T','e','s','t','2'};
uint8_t adv_bag3[] = {0x02,0x01,0x06,0x10,0x09,'M','i','n','e','w','-','B','L','E','-','T','e','s','t','3'};
uint8_t adv_bag4[] = {0x02,0x01,0x06,0x10,0x09,'M','i','n','e','w','-','B','L','E','-','T','e','s','t','4'};
uint8_t adv_bag5[] = {0x02,0x01,0x06,0x10,0x09,'M','i','n','e','w','-','B','L','E','-','T','e','s','t','5'};
uint8_t adv_bag6[] = {0x02,0x01,0x06,0x10,0x09,'M','i','n','e','w','-','B','L','E','-','T','e','s','t','6'};
 
uint8_t * adv_bag[] = {adv_bag1,adv_bag2,adv_bag3,adv_bag4,adv_bag5,adv_bag6};
 
uint16_t adv_interval[] = {500,900,1000,2000,2000,300};
 
uint16_t adv_timeout[] = {30000,30000,20000,60000,60000,40000};
 
void adv_test(void){
 
	uint8_t status;
 
	status = aci_hal_set_tx_power_level(0, 24);
		 if (status != BLE_STATUS_SUCCESS) {
		 PRINTF("aci_hal_set_tx_power_level() failed:0x%02x\r\n", status);
		 }
 
	 for(uint8_t i=0;i<6;i++){
 
	 /* adv paraments setting */
	 status = aci_gap_set_advertising_configuration(
	 		i,
	 GAP_MODE_GENERAL_DISCOVERABLE,
	 ADV_PROP_CONNECTABLE | ADV_PROP_SCANNABLE | ADV_PROP_LEGACY,
	 MSEC_TO_UNITS(adv_interval[i], UNIT_0_625_MS),
	 MSEC_TO_UNITS(adv_interval[i], UNIT_0_625_MS),
	 ADV_CH_ALL,
	 0,
	 NULL,
	 ADV_NO_WHITE_LIST_USE,
	 0, /* 0 dBm */
	 LE_1M_PHY, /* Primary advertising PHY */
	 0, /* 0 skips */
	 LE_1M_PHY, /* Secondary advertising PHY. Not used with legacy advertising. */
	 0, /* SID */
	 0 /* No scan request notifications */);
	 if (status != BLE_STATUS_SUCCESS) {
	 PRINTF("Error in aci_gap_set_advertising_configuration 0x%02x\r\n", status);
	 } else {
	 PRINTF("aci_gap_set_advertising_configuration() --> SUCCESS\r\n");
	 }
 
	 status = aci_gap_set_advertising_data(i, ADV_COMPLETE_DATA, sizeof(adv_bag1), adv_bag[i]);
	 if (status != BLE_STATUS_SUCCESS) {
	 PRINTF("Error in aci_gap_set_advertising_data 0x%02x\r\n", status);
	 }
 
	 adv_paraments[i].Advertising_Handle = i;
	 adv_paraments[i].Duration = 0;
	 adv_paraments[i].Max_Extended_Advertising_Events = 0;
 
	 }
 
 status = aci_gap_set_advertising_enable(ENABLE, 6, adv_paraments);
	 if (status != BLE_STATUS_SUCCESS) {
	 PRINTF("aci_gap_set_advertising_enable(NO_WHITE_LIST_USE) failed:0x%02x\r\n", status);
	 }
}

​

    This topic has been closed for replies.