Skip to main content
EShei.1
Associate
Jul 7, 2022 10:27 AM UTC
Question

Can I achieve long range reception of Bluenrg-355MT with a ceramic chip antenna?

Hello! I'm using module Bluenrg-355MT in my project. There is the antenna ACAG0801-2450-T on my board. This antenna transmits enough over a long distance (D>250m). But reception of this antenna is not more than 15m. Is it possible to achieve long range reception with such type of antennas? Have you tested this module with small size chip antennas? Thanks in advance!

    This topic has been closed for replies.

    2 replies

    Andrew Neil
    Super User
    Jul 7, 2022 10:36 AM UTC

    With antennas, size matters.

    To maximise range, you're going to need the best antenna gain you can get.

    Also, it depends on the whole transmission path from end-to-end - see "Link Budget"

    "This antenna transmits enough over a long distance (D>250m). But reception of this antenna is not more than 15m"

    Sounds like the problem is at the other end - you need to turn the power up at the other end!

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Laurent LOUAZON
    ST Employee
    Jul 20, 2022 4:21 PM UTC

    Hello,

    Please also note that not only antenna gain matters.

    It is important to consider antenna matching to ensure proper impedance adaptation.

    In theory both RF SOC output and antenna input are 50ohms but in reality this is never the case.

    Two or three discretes components are usually enough to ensure this proper matching (and be sure your antenna will effectively radiates at 2.45GHz)

    Regards

    Laurent