Skip to main content
Mahendra Rana
Associate III
Jun 29, 2019 6:14 AM UTC
Question

Can any one share me test procedure for EMC & RED tests of spbtle-rf module?

As SPBTLE-RF module is already CE certified and I have its test reports also. But as a complete product we have to perform this tests again: -

1) As per EMC EN 301 489-1 V1.9.2 / EN 301 489-17 standard: -

a) Radiated Emission

b) Electrostatic Discharge 

2) As per RED EN 300 328 V2.1.1 standard: -

a) Transmitter unwanted emissions in the spurious domain

b) Receiver spurious emissions.

By the test report it is not clear that how EUT means SPBTLE-RF module is configure while this above test performed.

Our queries are: -

1) Can any one share me How this module is tested during above tests. Testing method we will follow as per standards but how module is tested or configured or communicating with other device while above test are perform?

2) How Radiated Emission test performed ? As in certificate snapshot it is not cleared.

3) How Transmitter Spurious test and Receiver spurious test performed? In which only BLE will either continuously transmit or receive signal at maximum output power.

4) Is it other devices like laptop or mobile used with EUT during test will not affect our test results? As this device will also emits some radiations while testing.

Please reply if any one knows about my queries....

    This topic has been closed for replies.

    2 replies

    Mahendra Rana
    Associate III
    Jul 2, 2019 10:34 AM UTC

    Can anyone help us on above queries??

    Tesla DeLorean
    Guru
    Jul 2, 2019 12:00 PM UTC

    For these types of queries you might want to start with the sales office and FAE responsible for your account. Some testing may occur with test labs or agencies you may have to contact with directly.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..