Skip to main content
Adalgiso
Associate III
Apr 23, 2021 8:00 AM UTC
Question

Bug in STSW-S2LP-DK in S2LP_Library in S2LPRadioGetSymClkRecoverInfo

Hi,

S2LPRadioGetSymClkRecoverInfo code should be like this (Fast Gain are located in tmpBuffer[1] and nottmpBuffer[ 0]).

/**

* @brief Return the clock recovery configuration

* @param xSSymClkRecInit pointer to the clock recovery struct to be filled with the clock recovery settings of the chip.

* @retval None.

*/

void S2LPRadioGetSymClkRecoverInfo(CRF_TRX_S2LP_HandleTypeDef* handle, SSymClkRecInit* xSSymClkRecInit)

{

 uint8_t tmpBuffer[2];

 S2LPSpiReadRegisters(handle, CLOCKREC1_ADDR, 2, tmpBuffer);

  

 xSSymClkRecInit->xSClkRecMode = (SClkRecMode)((tmpBuffer[0]&CLK_REC_ALGO_SEL_REGMASK)>>4);

 xSSymClkRecInit->cClkRecIGainSlow = tmpBuffer[0]&CLK_REC_I_GAIN_SLOW_REGMASK;

 xSSymClkRecInit->cClkRecPGainSlow = (tmpBuffer[0]&CLK_REC_P_GAIN_SLOW_REGMASK)>>5;

   

 xSSymClkRecInit->cClkRec16SymPostFlt = (SFunctionalState)((tmpBuffer[1]&CLK_REC_ALGO_SEL_REGMASK)>>4);

 xSSymClkRecInit->cClkRecIGainFast = tmpBuffer[1]&CLK_REC_I_GAIN_FAST_REGMASK;

 xSSymClkRecInit->cClkRecPGainFast = (tmpBuffer[1]&CLK_REC_P_GAIN_FAST_REGMASK)>>5;

  

}

    This topic has been closed for replies.