Skip to main content
vikrant more
Associate II
Apr 18, 2018 7:22 AM UTC
Question

#BluetoothMesh development using libBlueNRG_Mesh_CM0.a library

Posted on April 18, 2018 at 09:22

I planning to add BlueNRG-2 SoC in our product with &sharpBluetoothMesh feature.

But how many models, specified in Mesh Model specification I could add using lib_BlueNRG_Mesh_CM0.lib  ?

How much RAM is available for user app, after executing Bluetooth Mesh out of 24Kb ?

As per Bluetooth SIG specification, during provisioning there are 3 ways to do authentication of device -

1) input-oob

2) output-oob

3) static oob

What type of method, ST BlueNRG-Mesh APP is using during Provisioning ?

Is there any in details documentation which help developers to understand ST version of &sharpBLuetoothMesh ?

Can I provision node based on ST firmware using Silicon Labs Bluetooth Mesh App or &sharpmeshctl utility from Bluez 5.49 ?

##bluetoothmesh
This topic has been closed for replies.

9 replies

alok
Visitor II
Apr 24, 2018 8:03 AM UTC
Posted on April 24, 2018 at 10:03

Dear Vikrant,

Thanks for your interest in BlueNRG-2 SoC for #BluetoothMesh feature.

a. We supported Vendor model in release STSW-BNRG-Mesh v1.02.000. Added support for Generic Model in STSW-BNRG-Mesh v1.03.000

     Further Lighting model will be added soon in release v1.04.000

b. RAM usage is mentioned in Release notes, You can use more than 4KB for your application.

c. We are support no-oob provisioning

d. Documentation is available on

http://www.st.com/blemesh

e. We didn't try to provision our firmware with other Apps or meshctl utility

alok
Visitor II
Apr 24, 2018 10:05 AM UTC
Posted on April 24, 2018 at 10:05

http://www.st.com/blemesh

VK Verma
Associate III
Apr 29, 2018 10:01 AM UTC
Posted on April 29, 2018 at 10:01

Hi Alok,

Latest version of BlueNRG-Mesh (1.05.00) got crashed on click while tested on Android Oreo/ MotoZ-2 Force.

Although earlier version was working on the same platform.   

0690X0000060Ap3QAE.png

Best Regards,

VK Verma