Skip to main content
Alexey_K
Visitor II
Aug 25, 2019 6:43 PM UTC
Question

BlueNRG2 timing adjustments for multiple connections

If I use the timings that are calculated in the "GET_Master_Slave_device_connection_parameters" if I try to connect to slave device error message 0x12. Can I see a correct example of settings for multiple connection?

This topic has been closed for replies.

1 reply

Winfred LU
ST Employee
Aug 27, 2019 1:53 AM UTC

Please refer to documents

  • Multiple Connection Guidelines

file:///C:/Program%20Files%20(x86)/STMicroelectronics/BlueNRG-1_2%20DK%203.1.0/Docs/Multiple_Connection_Guidelines/Multiple_Connection_Guidelines.html

  • Multiple Connection Formula

file:///C:/Program%20Files%20(x86)/STMicroelectronics/BlueNRG-1_2%20DK%203.1.0/Docs/Multiple_Connection_Formula/Multiple_Connections_Formula.html

A Multiple Connection Formula Timings Chart spreadsheet is provided for you to emulate the formula calculation and to determine the multiple connections parameters values for your specific application scenario:

file:///C:/Program%20Files%20(x86)/STMicroelectronics/BlueNRG-1_2%20DK%203.1.0/Docs/Multiple_Connection_Formula/Multiple_Connection_Formula_Timings_Chart.xlsx