Skip to main content
Francesco Sarasini
Associate II
Nov 28, 2018 9:52 AM UTC
Question

Bluenrg2 eeprom

Hi,

I'm trying to interface this eeprom with Bluenrg2 

http://ww1.microchip.com/downloads/en/DeviceDoc/Atmel-8828-SEEPROM-AT24CM02-Datasheet.pdf

I can write correctly. I can read 1 byte at time correctly. Trying to read more than 1 bytes results in incorrect readed data. 

when dataLen=1, read works correctly.

when dataLen>1, read returns incorrect data

bool Board_i2cReadEeprom(uint8_t deviceAddr, uint32_t position, uint8_t* data, uint8_t dataLen) {
 
	I2C_TransactionType t;
	uint32_t ii = 0;
 
	deviceAddr |= (position >> 16);
 
	Log_debug("Board", "reading");
	Log_debug("Board", "deviceAddr: %d", deviceAddr);
	Log_debug("Board", "position: %"PRIu32" ", position);
 
	t.Operation = I2C_Operation_Write;
	t.Address = deviceAddr;
	t.StartByte = I2C_StartByte_Disable;
	t.AddressType = I2C_AddressType_7Bit;
	t.StopCondition = I2C_StopCondition_Disable;
	t.Length = 2;
 
	I2C_FlushTx((I2C_Type*) BOARD_I2C);
	while (I2C_WaitFlushTx((I2C_Type*) BOARD_I2C) == I2C_OP_ONGOING) {
		if (ii++ > 1000000) {
			ii = 0;
			Log_error("Board", "i2c read1 timeout");
			return false;
		}
	}
 
	Board_i2c_eot = RESET;
	I2C_BeginTransaction((I2C_Type*) BOARD_I2C, &t);
 
	I2C_FillTxFIFO((I2C_Type*) BOARD_I2C, position >> 8);
	I2C_FillTxFIFO((I2C_Type*) BOARD_I2C, position);
 
	do {
		if (I2C_GetStatus((I2C_Type*) BOARD_I2C) == I2C_OP_ABORTED) {
			Log_error("Board", "i2c read op aborted");
			return false;
		}
 
		if (ii++ > 1000000) {
			ii = 0;
			Log_error("Board", "i2c read2 timeout");
			return false;
		}
	} while (Board_i2c_eot == RESET);
 
	while (!Board_i2cIsReady(deviceAddr)) {
		Board_wait(1);
	}
 
	t.Operation = I2C_Operation_Read;
	t.Address = deviceAddr;
	t.StartByte = I2C_StartByte_Disable;
	t.AddressType = I2C_AddressType_7Bit;
	t.StopCondition = I2C_StopCondition_Enable;
	t.Length = dataLen;
 
	Board_i2c_eot = RESET;
	I2C_BeginTransaction((I2C_Type*) BOARD_I2C, &t);
 
	do {
		if (I2C_GetStatus((I2C_Type*) BOARD_I2C) == I2C_OP_ABORTED) {
			Log_error("Board", "i2c read op aborted");
			Log_error("Board", "cause: %"PRIu32" ", ((I2C_Type*) BOARD_I2C)->SR_b.CAUSE);
			return false;
		}
 
		if (ii++ > 1000000) {
			ii = 0;
			Log_error("Board", "i2c read3 timeout");
			return false;
		}
	} while (Board_i2c_eot == RESET);
 
	for (uint8_t i = 0; i < dataLen; i++) {
 
		*data = I2C_ReceiveData((I2C_Type*) BOARD_I2C);
		data++;
	}
 
	return true;
}
 
void I2C2_Handler(void) {
 
	I2C_ClearITPendingBit((I2C_Type*) BOARD_I2C, I2C_IT_MTD | I2C_IT_MTDWS);
	Board_i2c_eot = SET;
}

This topic has been closed for replies.

1 reply

Winfred LU
ST Employee
Feb 21, 2019 6:23 AM UTC

Hi Francesco,

Could you provide the traces for I2C bus?

The function looks fine to me, except that i don't quite understand the reasons for line 47-49.

	while (!Board_i2cIsReady(deviceAddr)) {
		Board_wait(1);
	}

Thank you.

Best Regards,

Winfred