Skip to main content
ann
Visitor II
Aug 7, 2019 10:44 PM UTC
Question

BLUENRG2 data transmission& data length extension¬ification

i am able to send 20 bytes to an android app through the following codes when the android app executes command: bluetooth_gatt.readCharacteristic(gattChar);

:

void aci_gatt_read_permit_req_event(uint16_t Connection_Handle,

                  uint16_t Attribute_Handle,

                  uint16_t Offset)

{

uint8_t send1[] = {0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,

0x31,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,};

if (aci_gatt_update_char_value_ext(Connection_Handle,envSensServHandle,tempCharHandle,0,20,0,20,(uint8_t *)send_to)==BLE_STATUS_SUCCESS){

aci_gatt_allow_read(Connection_Handle);

  };

my question is :

if it is possible to achieve that the andriod app keep reading and bluenrg2 keep sending data? and if it is possible to get ride of aci_gatt_allow_read(Connection_Handle);

how to achieve send 247 data at once? the data sheet says it is possible, but i couldn't find and instruction about it.

QUESTION 2:

the following are the andriod code to enable notification, but when i send a notification through aci_gatt_update_char_value_ext, the android app didn't enter the callback relating to notification received.

bluetooth_gatt.setCharacteristicNotification(gattChar, enabled);

BluetoothGattDescriptor descriptor = gattChar.getDescriptor(UUID.fromString("00002904-0000-1000-8000-00805f9b34fb"));

// 00002904-0000-1000-8000-00805f9b34fb are get from the following code:

//for (BluetoothGattDescriptor descriptor:gattChar.getDescriptors()){

// Log.e(Constants.TAG, "BluetoothGattDescriptor: "+descriptor.getUuid().toString());

// }

descriptor.setValue(BluetoothGattDescriptor.ENABLE_NOTIFICATION_VALUE);

boolean ok = bluetooth_gatt.writeDescriptor(descriptor);

This topic has been closed for replies.