Skip to main content
LJ.1
Associate
Jan 8, 2022 8:53 AM UTC
Question

bluenrg2 always crash with ac contactor

i use bluenrg2 as main mcu , to control a ac 220v ac contactor , the main logic is

bluenrg2 -> Optocoupler -> DC 12V relay -> AC 220V ac contactor

If i open/close, the bluetooth will disconnect and will crash very often. Is it not suitable for my case

    This topic has been closed for replies.

    3 replies

    Andrew Neil
    Super User
    Jan 8, 2022 10:37 PM UTC

    Sounds like an EMC fail - your design is over susceptible to conducted and/or radiated disturbances from the contactor and/or the load switching.

    Start by looking carefully at your supply lines:

    • are they noisy?
    • are they drooping/spiking?
    • etc ...
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    LJ.1
    LJ.1Author
    Associate
    Jan 9, 2022 1:33 PM UTC

    could you help me to check the schematic?

    Andrew Neil
    Super User
    Jan 10, 2022 12:52 AM UTC

    You'll have to post the schematic if you want people to check it.

    And it's not just about the schematic, the layout is also important - so you'll also need to post some good, clear, in-focus photographs of your setup.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.