Skip to main content
dimitar
Associate
Dec 10, 2014 6:41 AM UTC
Question

BlueNRG Set Advertising Data

Posted on December 10, 2014 at 07:41

Hi,

I'm trying to set the advertising data and make it advertise, but the client doesn't detect any of the data.

Here are the command that I use:

HCI_LE_Set_Advertizing_Parameters

HCI_LE_Set_Random_Address

HCI_LE_Set_Advertizing_Data

HCI_LE_Set_Advertize_Enable

What am I missing?

Thanks
This topic has been closed for replies.

1 reply

marchese.graziella
Visitor II
Dec 11, 2014 9:47 AM UTC
Posted on December 11, 2014 at 10:47

Hi Dimitar,

Using the commands below, the client device should be able to see the device.

Anyway, could you tell me which parameters are used?

Regards,

Graziella