Skip to main content
enrico239955_stm1
Associate
Nov 17, 2015 6:10 PM UTC
Question

bluenrg MS setup ok, but no connetion established

Posted on November 17, 2015 at 19:10

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This topic has been closed for replies.

2 replies

marchese.graziella
Visitor II
Nov 18, 2015 3:20 PM UTC
Posted on November 18, 2015 at 16:20

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6X1&d=%2Fa%2F0X0000000bq3%2FhhjrTWflz7Wos.tbz6PkPumombwnV1RBrQzOSBXdqmw&asPdf=false
enrico239955_stm1
Associate
Nov 19, 2015 2:33 PM UTC
Posted on November 19, 2015 at 15:33

Thanks for the reply.

From another post I already knew the changes on fw 7.1

But with the help of another colleague I discovered that the problem was a too short time settings for HS_Startup_Time. It worked fine with the evaluation board, but with the new custom board, I had to change it to 1.4ms. Now the board is seen by other devices almost immediately and can exchange data with them.

In the application notes, indeed was written that a too short time would make impossible to send/receive packet (even if it is not put in evidence enough in my opinion, I would suggest a troubleshooting or FAQ with the common mistakes on the IFR configuration)