Skip to main content
hornyak.matedaniel
Associate
Apr 29, 2019 11:26 AM UTC
Question

Bluenrg-ms in simultaneous central/peripheral mode hangs

I would like to use Bluenrg-ms in simultaneous central/peripheral mode. My initialization method builds up like this: 1. after the first reset, set up stack mode 3 by calling aci_hal_wirite_config data, 2. call aci_gap_init_IDB05A1 function with peripheral and central simultaneous mode, 3. try to call aci_gap_start_general_discovery_proc(0x10,0x10,PUBLIC_ADDR,0x00); and it returns successfully but hci event callback hangs and IRQ pin stays high. I use X-CUBE-BLE1.4.2.0 additional software package and firmware 7.2. Could anybody help me solve this problem?

This topic has been closed for replies.

2 replies

solomonviveros
Associate II
Jun 10, 2020 4:52 PM UTC

Were you able to make any progress in solving your issue of the BlueNrg-MS hanging when in simultaneously scanning/advertising? I'm running into a similar issue though I'm using mode 4, with passive observing, rather than doing a general discovery...I'm finding the IRQ line to stay high and am unable to clear the IRQ without a reset...

hornyak.matedaniel
Associate
Jun 11, 2020 5:43 AM UTC
Helo! Yes I have solved this problem but not sure how because more than a year passed since I asked this question. As I remember it was something in connection with interrupt settings and some soldering problem. Regards ST Community ezt írta (időpont: 2020. jún. 10., Sze 18:52):