Skip to main content
ZSara
Visitor II
Oct 12, 2018 6:36 AM UTC
Question

BlueNRG-MS data throughput

Hi,

I'm fighting with a low data throughput of the BlueNRG-MS. The BlueNRG based device acts as a peripherial and sends notifications periodicaly to PC or Android app. The problem is I'm not able to achieve a higher data rate than approx. 1 kB per second. BLE frame data size is 20 bytes.

How should I increase the data speed? I think the way is sending multiple packets within one connection interval but I don't know how to do this. Or is there another way?

Thanks a lot

Zdenek

    This topic has been closed for replies.

    2 replies

    rdscliff
    Associate III
    Oct 19, 2018 5:47 PM UTC

    I was fighting the same problem a while ago. Here are the things we did to get the throughput up and get multiple packets sent in one connection interval:

    • Don't wait for the command complete for each characteristic update. Just send the next one. BUT, you must make sure you handle the error code in command complete for Insufficient Resources. This means you sent too much and will have to resubmit the characteristic update.
    • Rotate characteristic updates through several characteristics. I didn't come up with this but another engineer said this increased throughput. Instead of sending 4 characteristic updates to one characteristics, send one to characteristic 1, the second to characteristic 2, etc.

    Using these techniques, I was able to observe 2 to 4 packets sent per connection interval with a Bluetooth protocol analyzer.

    If you need even more throughput, consider going to BlueNRG-2 with its higher MTU. With one big characteristic update, the L2CAP on the chip figures out how to pack the connection interval.

    Associate
    Nov 21, 2024 8:36 AM UTC

    Hello,

     

    I'm trying to achieve the same thing for a "SPBTLE-RF" module on a B-L475E-IOT01A2 Discovery Kit which is based on BluneNRG-ms. I'm trying to achieve a total baud rate of about 256 kbps. 
    I've tried multiple approaches like breaking the data down to multiple characteristics but I was not able to go higher than about 16kbps. However, in the datasheet for BlueNRG-ms, it says that the "Data Rate" can go up to 1 Mbps. I'm so confiused.

     

    I would appreciate it if you could guide me in the right direction.