Skip to main content
daniele2399
Associate II
Feb 14, 2017 10:35 AM UTC
Question

BlueNRG-MS connection interval

Posted on February 14, 2017 at 11:35

Hi,

I'm using the BlueNRG-MS chipset. As far as I've understood, the connection interval is set through 'aci_gap_set_discoverable' and if the related arguments of the function (SlaveConnIntervMin and SlaveConnIntervMax) are 0, it is set to 7.5 ms (as for BLE standard), otherwise it is set using multiples of 1.25 ms. Which is the minimum value which can be set? Can the connection interval be set to 1.25 ms in order to maximize throughput?

Thank you,

Daniele

#bluenrg-ms
    This topic has been closed for replies.

    1 reply

    Antonio Vilei
    ST Employee
    Feb 15, 2017 9:13 AM UTC
    Posted on February 15, 2017 at 10:13

    Hi Daniele,

    the minimum value for the connection interval is 7.5 ms. As you said, it is set in multiple of 1.25 ms, but you can't go any lower than 7.5 ms. Also, please notice that the actual connection interval that will be used is chosen by the master.