Skip to main content
allard
Senior
Nov 1, 2019 1:43 PM UTC
Question

blueNRG Master/Central Library conn_length

I'm working on a central BLE device. I'm having some trouble with the sensor and the hub not being in sync. It looks like that the central device wakes up to late, every 3rd wake event the central wakes up at the right time and a PDU is sent/received correctly(connection latency is zero).

I'm currently checking all the connection parameters, and came across the min_conn_length and max_conn_length fields in the struct connDevType of the Master/Central Library. Anyone knows what these parameters mean, the documentation is way to brief? Any other thought what could cause the wakeup desync (using internal RO)?

This topic has been closed for replies.