Skip to main content
AndyR1
Senior
February 6, 2024
Question

bluenrg-lp deepstop, WakeupFromSleepFlag prevents from power save mode, all wakeup source are reset

  • February 6, 2024
  • 2 replies
  • 1145 views

Hello,

I'm using bluenrg-lp with BLE stack initialized for Rx only, I set to GAP_OBSERVER_ROLE and the observation procedure is stopped, I'm trying to enter in sleep mode POWER_SAVE_LEVEL_STOP_WITH_TIMER based on example code :

 

WakeupSourceConfig_TypeDef wakeupIO = {0, 0, 0, 0};
PowerSaveLevels stopLevel;
HAL_VTIMER_Tick();
BLE_STACK_Tick();
NVMDB_Tick();
HAL_PWR_MNGR_Request(POWER_SAVE_LEVEL_STOP_WITH_TIMER, wakeupIO, &stopLevel);
printf("Exit from sleep mode %d.\r\n", stopLevel);

 

I added print in HAL_PWR_MNGR_Request() function :

 

final_level : 2, app_powerSave_level : 3, level : 2
final_level : 2, vtimer_powerSave_level : 2
final_level : 2, pka_level : 3
Exit from sleep mode 0.

 

It shows that the three parts agree for level 2 sleep mode but the final in 0 (RUN mode).

It goes in this condition (in HAL_PWR_MNGR_Request()) :

 

/* If for some reason the power save is skipped (i.e. wakeup source already active.....) */
if (RAM_VR.WakeupFromSleepFlag == 0) {
 final_level = POWER_SAVE_LEVEL_RUNNING;

 

 The "WakeupFromSleepFlag" is set to 1 only before main() is called.

How to get this variable to 1 ? or How to prevent this variable from going to 0 ?

Thanks

This topic has been closed for replies.

2 replies

AndyR1
AndyR1Author
Senior
February 8, 2024

WakeupFromSleepFlag is set to 0 at the start of HAL_PWR_MNGR_Request() and WakeupFromSleepFlag is set to 1 only from startup_BlueNRG_LP.c :

int __low_level_init(void) 
{
 /* If the reset reason is a wakeup from DEEPSTOP restore the context */
 if ((RCC->CSR == 0) && ((PWR->SR1 != 0)||(PWR->SR3 != 0))) {
 RAM_VR.WakeupFromSleepFlag = 1; /* A wakeup from DEEPSTOP occurred */

CSR bits is set to 1 if a reset occured (RM0479 6.6.14), SR1 and SR3 bits are set to 1 if a wakeup occured (RM0479 5.6.5).

I also print before and after HAL_PWR_MNGR_Request() output of HAL_PWR_MNGR_WakeupSource() function which is SR1 and SR3 registers in a 32 bits value, all bits are 0.

From these elements, I understand that I can't get a deepstop mode because there was no wakeup before ?

AndyR1
AndyR1Author
Senior
February 14, 2024

hello @Sebastien DENOUAL 

Could you help me to understand how "WakeupFromSleepFlag"  works please ? and why RAM_VR.WakeupFromSleepFlag is reset ?