Associate
Nov 10, 2022 3:15 PM UTC
Question
BlueNRG-LP Current Consumption
- 2 replies
- 1240 views
Hi, I am evaluating the current consumption of BlueNRG-LP using STEVAL-IDB10V1 and i am a bit confused with the expected and actual device's currents.
According to the datasheet, peak TX current during connection at 0dB is 4.3mA, according to Current Consumption Estimation tool it is 5.43mA and in my measurements i get 5.6mA.
For peak RX current, datasheet specifies 3.4mA, in Current Consumption Estimation tool its 3.73mA and in my measurements i get 5.6mA (same as TX).
Any idea why the difference especially between the datasheet and the estimation tool? Which value should i expect?