Skip to main content
dario2
Associate II
Oct 9, 2015 10:31 AM UTC
Question

BlueNRG: does it support Prepare Write reception?

Posted on October 09, 2015 at 12:31

Hello,

we have to transfer long attributes (images) on BlueTooth.

We read in BLE Specifications 4.0 that this can be accomplished

using the “Write Long Characteristic Values�? procedure described in 4.9.4 of part F:

a sequence of Attribute Protocol

Prepare Write Request – Prepare Write Response

terminated by:

Execute Write Request - Execute Write Response

However, looking at the code, it seems that only BlueNRG MS (and not BlueNRG)

provides the offset:

#define EVT_BLUE_GATT_ATTRIBUTE_MODIFIED          (0x0C01)

typedef __packed struct _evt_gatt_attr_modified{

  uint16_t conn_handle; /**< The connection handle which modified the attribute. */

  uint16_t attr_handle; /**< Handle of the attribute that was modified. */

  uint8_t  data_length; /**< The length of the data */

#if BLUENRG_MS

///@cond BLUENRG_MS

  uint16_t offset;     /**< Offset from which the write has been performed by the peer device */

///@endcond

#endif

  uint8_t  att_data[VARIABLE_SIZE]; /**< The new value (length is data_length) */

} PACKED evt_gatt_attr_modified;

What happens when a prepare write is received by the BlueNRG?

Is EVT_BLUE_GATT_ATTRIBUTE_MODIFIED event generated or is command rejected?

 Does evt_gatt_attr_modified contain at least length and data?

I also wonder why an uint8_t (max value = 255) is used for data_length,

as in“BlueTooth_Core_v4.0 “ Volume 3 of Part F – Attribute Protocol (ATT)

section 3.2.9 ''Long Attribute Values'' I read:

“The maximum length of an attribute value shall be 512 octets.�?

Thanks

This topic has been closed for replies.