Skip to main content
SPopo
Visitor II
Feb 26, 2020 10:49 AM UTC
Question

BlueNRG-2 - how to switch on the LS RO oscillator with working LS XO oscillator without external reset (RESETn pin) or power cycling after firmware updating over "OTA"? The chip is BlueNRG-232 (it reports a "chip version" 1.0.0).

We use BlueNRG-2 in custom sensor. The original firmware uses LS XO (32 kHz crystal). But we need to have ability to choose the LS "RO" or "XO" after firmware updating over "OTA" (FOTA). It seems that if LS XO has been turned on once then the LS RO is turned off up to power cycling or external reset. Is there some way to handle this issue using only internal reset and some program code?

Clarification, we want to switch "LS XO" to "LS RO" but we cannot switch it (without an external reset or power cycling). Can anybody help us?

    This topic has been closed for replies.