Skip to main content
Visitor II
Oct 18, 2024 12:25 PM UTC
Question

BlueNRG-2 ADV_DIRECT_IND examples

Hallo,

So I have this ADV_IND advertisement mode, which works just fine:

 

 

 

 // Advertising definitions
 ret = aci_gap_set_discoverable(ADV_IND, // Connectable undirected advertising
 (ADV_INTERVAL_MIN_MS * 1000)/625, // Minimum advertising interval
 (ADV_INTERVAL_MAX_MS * 1000)/625, // Maximum advertising interval
 STATIC_RANDOM_ADDR, // Random device address
 NO_WHITE_LIST_USE, // Advertising filter policy
 sizeof(local_name), // Length of the local_name field in octets
 local_name, // Local name of the device
 0, // Length of the Service Uuid List in octets
 NULL, // List of the UUIDs
 0, // Minimum value for slave connection interval (NaN)
 0); // Maximum value for slave connection interval (NaN)
 
 if (ret != BLE_STATUS_SUCCESS)
 {
 ActiveState = BLEState_ERROR;
 TargetState = BLEState_ERROR;
 BLE_DRIVER_TRACE("Device set discoverable not accepted. Error = 0x%02x", ret);
 return;
 }

 

 

 

I would like to understand how to take a paired device and attempt to directly advertise to that using the ADV_DIRECT_IND mode, but I cannot find any examples of that and just exchanging ADV_IND above to ADV_DIRECT_IND results in an BLE_STATUS_INVALID_PARAMS error, which I guess makes sense as I have not defined what device I want to target my advertisement at.

Sooo, is there an example of how to setup the ADV_DIRECT_IND advertisement mode?

Also, what does this mean in practice? I assume other devices scanning for BLE advertisements will not "see" this advertisement at all then? Technically there will be an advertisement sent out, but in practice I assume it is filtered by any device for which it is not targeted?

 

This topic has been closed for replies.