Skip to main content
jaylong
Associate II
Sep 10, 2019 10:03 PM UTC
Solved

BlueNRG-2 5.0 long range support via lower bit rate

Hi,

The BlueNRG-2 describes compatibility with the 5.0 spec. but I've been unable to find specific mention of the longer range via lower bit rate 500kbps or 125kbps and Forward Error Correction (FEC).

Is this long range mode supported and if so can you point me to some documentation?

Thanks!

jay

This topic has been closed for replies.
Winfred LU
Winfred LUBest answer
ST Employee
Sep 11, 2019 7:07 AM UTC

500 kbps and 125 kbps (coded PHY) is not supported for BlueNRG-2.

Thank you.

3 replies

Winfred LU
Winfred LUBest answer
ST Employee
Sep 11, 2019 7:07 AM UTC

500 kbps and 125 kbps (coded PHY) is not supported for BlueNRG-2.

Thank you.

jaylong
jaylongAuthor
Associate II
Sep 11, 2019 2:43 PM UTC

Thanks Winfred,

Do you know if there are any plans to enable this feature through firmware updates?

Thanks

jay

Winfred LU
ST Employee
Sep 12, 2019 3:15 AM UTC

Hi Jay,

Hardware modification is required to support the LE coded PHY.

The plan is to support both of them in the next generation of BlueNRG SoC : BlueNRG-LP, which is expected to be ready this year.

Best Regards,

Winfred