Skip to main content
Nav Dev
Associate II
Feb 23, 2017 12:00 PM UTC
Question

BlueNRG-1 run debug, combine with cc1310

Posted on February 23, 2017 at 13:00

Hi ST,

I am working with the BlueNRG-1 using STEVAL_IDB and i have few questions please:

1- When i program some ST BLE via using Navigatorv2.3.0, the main code not the BLE stack, where it saved? in the main MCU or the NRG-1?

2- I want to combine the NRG-1 with TI sub1-GHZ cc1310(Backward compatibility), so i have few questions in this area:

2.1 - Where the code that related to the BLE must run? on the cc1310 or NRG-1?

2.2 - Did it possible to configure and send commands to the NRG-1 via other MCU? if yes i would be happy if you share some example, reference ...

3- Did there is some tool develop/debug with the 

BlueNRG-1 code example, and it's free?

4- What is the best IDE that you recommended to work with the BlueNRG-1?

Thanks.

#bluenrg-1
    This topic has been closed for replies.

    2 replies

    ST Technical Moderator
    Feb 23, 2017 3:21 PM UTC
    Posted on February 23, 2017 at 16:21

    Hi,

    You may refer to the User manualsand related Tools/softwarein the

    http://www.st.com/content/st_com/en/products/wireless-connectivity/bluetooth-bluetooth-low-energy/bluenrg-1.html

    .

    The BlueNRG GUI is available in

    /external-link.jspa?url=https%3A%2F%2Fmy.st.com%2Fcontent%2Fmy_st_com%2Fen%2Fproducts%2Fembedded-software%2Fwireless-connectivity-software%2Fstsw-bnrgui.license%3D1487062354html

    .

    Hope this helps you.

    0690X00000606F2QAI.png

    Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Nav Dev
    Nav DevAuthor
    Associate II
    Mar 8, 2017 11:00 AM UTC
    Posted on March 08, 2017 at 11:00

    Thanks 

    Imen D for responding, 

    After looking to the references that you advice to me, i have few question please:

    As i mentioned before, we want to use TI cc1310 for SUB1-GHz and the NRG-1 for BLE, there is 2 ways (that i know about):

    1- Connect the NRG-1 to the cc1310 via SPI and send ACI commands.

    2- Set the NRG-1 as a Stand Alone, and share some memory between the cc1310 and the NRG-1 for logic's and others...

    Q1: did the ACI commands have full control of the BLE stack as the Stand Alone?

    Q2: What is the best way, the first way or the second?

    Q3: Did there is another way that o didn't mentioned?

    Any other advice in this topic will be welcome.