Skip to main content
Adriana Albert
Associate
Oct 5, 2017 8:47 AM UTC
Solved

BlueNRG-1 extended packet length

Posted on October 05, 2017 at 10:47

I am evaluating the use of the SPBTLE-1S module, based on BlueNRG-1 and Bluetooth v4.2 compilant, to interact with iOS. BLE 4.2 specification includes data length extension feature which improves throughput and reduces transaction time. However, according to documentation, only BlueNRG-2 supports BLE extended packet length feature. 

Is it possible to upgrade BLE stack embedded software (

library managing the RF part

) with a version wich 

extends the possible MTU size up to 158 bytes?

Thank in advance.

This topic has been closed for replies.
Antonio Vilei
Antonio VileiBest answer
ST Employee
Oct 9, 2017 1:07 PM UTC
Posted on October 09, 2017 at 15:07

Dear Adriana Albert,

as reported in the documentation, only BlueNRG-2 supports the BLE extended packet length and there are no firmware updates available to enable this feature with BlueNRG-1 too.

1 reply

Antonio Vilei
Antonio VileiBest answer
ST Employee
Oct 9, 2017 1:07 PM UTC
Posted on October 09, 2017 at 15:07

Dear Adriana Albert,

as reported in the documentation, only BlueNRG-2 supports the BLE extended packet length and there are no firmware updates available to enable this feature with BlueNRG-1 too.