BlueNRG-1 ADC input with higher voltage than VBAT sinks a lot of current
According to the datasheet, it is possible with ADC to sample voltage up to 3.6V, even with lower VBAT, if proper attenuator.
I'm powering the MCU with 2.5V and feeding battery (up to 3.6V) to ADC1 pin. No matter what setting I use, the ADC is still sinking a lot of current - approx. 40 uA for ADC1 pin and more than 1 mA for ADC2 pin.
I've even tried setting CHSEL to 0 that should result in input connected to the ADC, but it is still the same.
My standard setup is ADC1, CHSEL=2, OSR=0, single mode, REFSEL=2, PGASEL=2.
Is there anything I'm missing in the specs?