Skip to main content
dnedov
Visitor II
Nov 13, 2015 11:50 AM UTC
Question

BlueNR-MS Active

Posted on November 13, 2015 at 12:50

Hi all!

Please, can you help me. I have next problem. In My device I use BlueNRG-MS (HSI-16MHz, LSE ext - 32.768). BlueNRG init Ok, but not available in RF.  He is active with a period of 30 seconds (name ''atn_B41'')

0690X00000602dxQAA.jpg

But, then I made CS on SPI active (set ''0'') - BlueNRG-MS - active all time

0690X00000602e2QAA.jpg

Code init module:

''

main(){

....

getBlueNRGVersion(&hwVersion,&fwVersion);

    printk(''hwVersion = 0x%X fwVersion = 0x%X'',hwVersion,fwVersion);

    /* Reset BlueNRG hardware */

    BlueNRG_RST();

    wait_IRQ_SPI_FLAG();

  Osal_MemCpy(bdaddr, SERVER_BDADDR, sizeof(SERVER_BDADDR));

  ret = aci_hal_write_config_data(CONFIG_DATA_PUBADDR_OFFSET,CONFIG_DATA_PUBADDR_LEN,bdaddr);

  ret = aci_gatt_init();

  ret = aci_gap_init(GAP_PERIPHERAL_ROLE, 0, 7, &service_handle, &dev_name_char_handle, &appearance_char_handle);

  //appearance_char_handle - 8;

  //service_handle  - 5;

  //dev_name_char_handle - 6;

  aci_gatt_update_char_value(service_handle, dev_name_char_handle, 0,strlen(name), (uint8_t *)name);

  ret = aci_gap_set_auth_requirement(MITM_PROTECTION_REQUIRED,OOB_AUTH_DATA_ABSENT,0, 7,16,USE_FIXED_PIN_FOR_PAIRING,123456,BONDING);

  ret = Add_Acc_Service();

  ret = Add_Environmental_Sensor_Service();

 ret = aci_hal_set_tx_power_level(1,4);

while(1)

{

      HCI_Process();

      User_Process(&axes_data);

    }

...

}

....

void setConnectable(void)

{  

  tBleStatus ret;

  

  const char local_name[] = {AD_TYPE_COMPLETE_LOCAL_NAME,'a','t','n','_','B','4','1'};

  /* disable scan response */

  hci_le_set_scan_resp_data(0,NULL);

  printk(''General Discoverable Mode.\n'');

  

  ret = aci_gap_set_discoverable(ADV_IND, 0, 0, PUBLIC_ADDR, NO_WHITE_LIST_USE,

                                 sizeof(local_name), local_name, 0, NULL, 0, 0);

  printk_co(GREEN,''aci_gap_set_discoverable() ret=0x%X'',ret);

  if (ret != BLE_STATUS_SUCCESS) {

      printk(''Error while setting discoverable mode (%d)\n'', ret);

  

  }  

}

''

#avalible #init #bluenrg-ms
This topic has been closed for replies.