Skip to main content
brent239955
Visitor II
May 7, 2016 12:51 AM UTC
Question

BLE client retrieve device name and RSSI

Posted on May 07, 2016 at 02:51

Hello,

I'm developing code for the BlueNRG-MS device, in a central role. I'm wondering what API allows me to retrieve the advertising devices name and the packet RSSI?  I've initiated a discovery with aci_gap_start_general_discovery_proc() and receive the  EVT_LE_ADVERTISING_REPORT event, but its not clear how to retrieve the ''Device Name'' and RSSI.

Thank you,

Brent

#ble #rssi #bluenrg-ms #bluenrg
This topic has been closed for replies.

1 reply

hardware
Associate III
May 25, 2016 9:58 PM UTC
Posted on May 25, 2016 at 23:58

You need to read the data section of the  EVT_LE_ADVERTISING_REPORT event for the device's name. Data section will look something like: 0201060508426C7565020A08 that should be read according to Bluetooth specs as follow:

02 = size, 01 = type = flag, 06 = value of flag

05 = size, 08 = short name, 426C7565 = Blue in ascii

02 = size, 0A = remote RSSI, 08 = value

Caution this is the remote RSSI meaning the value on the emitter side.

If you want the value on the receiver side, you'll need to use the RSSI section of the EVT_LE_ADVERTISING_REPORT event.

Hope this helps