Skip to main content
AMACH.1
Associate
Aug 24, 2023 11:36 AM UTC
Question

Beacon discovery problem

Hello,

I have configured the BLE Beacon V1.0 sensor with the Nano Beacon software, I can detect it with applications like nrf Connect or ST BLE Toolbox. I've programmed a stm32 card as a client, I can detect the devices, but I can't detect the beacon sensor; that's the problem I'm having.

Here are screens showing the configuration I made with the Nano Beacon software:

 

 

AMACH1_5-1692876253934.jpegAMACH1_6-1692876261444.jpegHere are the functions I programmed on the stm32 board to detect the beacon:

AMACH1_7-1692876501396.png

with : 

#define SCAN_P 16384      

#define SCAN_L 16384

AMACH1_8-1692876580965.png

 

/********************************************************************************************/

 

Do you have any suggestions please?

Thanks in advance.

#Beacon

 

 

This topic has been closed for replies.