Skip to main content
Visitor II
Apr 20, 2026 12:17 PM UTC
Question

BALF-SPI2-02D3 datasheet stackup: what does “35 µm + 31 µm” mean?

I’m using BALF-SPI2-02D3 with the S2-LP at 433 MHz and have a question about Figure 13 in the datasheet.

The recommended PCB stackup shows:

  • Top plane: 35 µm + 31 µm
  • Mid layer: 31 µm
  • Bottom plane: 35 µm + 31 µm

What exactly does “35 µm + 31 µm” mean for the outer layers?

Is this:

  • base copper + plated copper,
  • finished copper thickness in ST’s stackup notation,
  • or something else?

I’m trying to choose a 1.0 mm, 4-layer PCB stackup from a commercial manufacturer and would like to match the recommendation as closely as possible.

Thanks for any clarification.

1 reply

Peter BENSCH
ST Technical Moderator
Aug 5, 2026 11:43 AM UTC

Welcome ​@cehmke, to the community!

I’m sorry that I didn’t see your question earlier, but I would still like to answer it regardless of its age: 35µm+31µm` is most likely meant as base copper + plated copper.

Regards
/Peter

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.