Skip to main content
JMic
Visitor II
Mar 13, 2022 12:29 PM UTC
Question

B-U585I-IOT02A board with external SD Card reader with FATFS

Hi, I have B-U585I-IOT02A board. I'd like to log data to an uSD card. Is it possible to connect external SD Card reader along with FATFS ? If so, which protocol to use SPI or MMC and which physical ports? I don't use onboard: gyroscope, magnetometer, lcd interface, touchscreen interface.

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Mar 13, 2022 12:55 PM UTC

One could perhaps check schematic vs data sheet to see if you've got any hope of exposing the SDMMC interfaces.

​

S​PI should at least be exposed on the Arduino rails.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..