Skip to main content
0x80
Associate
Jun 2, 2019 6:03 PM UTC
Question

Add a USB host port on a STM32F103 dev board

Hi,

I'm just starting out with embedded programming & electronics so please bear with me :)

I am starting a project based on the STM32F103 Nucleo board. The first thing I want to do is create a USB host port to connect a class-compliant MIDI device.

From this link I learned that means the USB class is likely OTG. What I don't understand yet is what I need in terms of hardware. I would like to use a USB type A port. Can I hook it up straight to the MCU pins on the dev board without additional ICs?

I ordered this book today which will surely help me with this, but it will take some days to arrive and I'd like to prepare already if I can.

    This topic has been closed for replies.

    4 replies

    0x80
    0x80Author
    Associate
    Jun 3, 2019 9:20 AM UTC

    I think I've learned two important things this morning:

    • Yes, USB data lines are connected directly to the pins. I could for example use this simple module.
    • The 103x processor do not support USB host.

    From what I've read here USB host / on-the-go class would require a 105/7 board at least. Luckily I didn't buy the hardware yet :)

    That's a bit of a bummer because I was going base my project on an open-source project which uses the 103. I guess I will have to put in a bit more effort to port that code/hardware design.

    But anyway, eventually my project requires both a USB host/OTG and a USB device port (also for MIDI) simultaneously. So I will first figure out that processor supports that...

    Explorer II
    May 7, 2024 4:26 PM UTC

    Hi,
    I am also having some trouble getting a USB breakout board connected to the Nucleo-F103RB, I only need the device in peripheral mode so not worried about otg, but I only get USB Device not recognised on my pc. I am still new to STM32 and this is the first time I am prototyping my own board for the chip, so I need to know how to communicate with the chip and instead of just buying the bluepill or similar as some have suggested for this issue. 

    Tesla DeLorean
    Guru
    May 7, 2024 10:21 PM UTC

    Pull a schematic for the board and look at how the USB connects to the STM32F103 providing the ST-LINK functionality

    Look at this, README.md explains wiring expectations

    https://github.com/STMicroelectronics/STM32CubeF1/tree/master/Projects/STM32F103RB-Nucleo/Applications/USB_Device/HID_Standalone

    And these you might port over 

    https://github.com/STMicroelectronics/STM32CubeF1/tree/master/Projects/STM3210E_EVAL/Applications/USB_Device

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..