Skip to main content
Associate II
Jul 30, 2025 5:45 AM UTC
Solved

Working with multiple STEVAL-EVK-U0I boards

Hi, 

I'm curious to see if it is possible to connect more than one STEVAL-EVK-U0I boards to a computer and read images of all of them? The SDK has  an init function that allows you give a board id, but it is unclear what the board id means or if it will give the desired effect. Any help is appreciated. 

 

Thanks

This topic has been closed for replies.
Jean_PoireBest answer
ST Employee
Jul 30, 2025 10:18 AM UTC

Hi @oaa3wf ,

It is indeed possible to use simultaneously more than one STEVAL-EVK-U0I boards. An id (starting from 0) is automatically attributed when more than one board is detected. You just have to define two sensor_dll object in the python script:

# # Init the board
first_sensor_dll = SensorDll(LIB_NAME, decode_frame)
first_sensor_dll.init_board(board_id=0)
second_sensor_dll = SensorDll(LIB_NAME, decode_frame)
second_sensor_dll.init_board(board_id=1)

 Best regards,

Jean

7 replies

Jean_PoireBest answer
ST Employee
Jul 30, 2025 10:18 AM UTC

Hi @oaa3wf ,

It is indeed possible to use simultaneously more than one STEVAL-EVK-U0I boards. An id (starting from 0) is automatically attributed when more than one board is detected. You just have to define two sensor_dll object in the python script:

# # Init the board
first_sensor_dll = SensorDll(LIB_NAME, decode_frame)
first_sensor_dll.init_board(board_id=0)
second_sensor_dll = SensorDll(LIB_NAME, decode_frame)
second_sensor_dll.init_board(board_id=1)

 Best regards,

Jean

oaa3wfAuthor
Associate II
Jul 30, 2025 5:45 PM UTC

Thanks @Jean_Poire . I'll give it a try.

oaa3wfAuthor
Associate II
Jul 30, 2025 11:06 PM UTC

So I gave this a try and got the following:

Loading st_brightsense_sdk_vdx6gx.dll
IMG platform version 305 loaded :)
Boards connected: (0,P4405C-00A#0306) (1,P4405C-00A#0310)
Board ID selected : 0
Initiating CCI communication at address 32
Sensor detected on interface 0
Loading st_brightsense_sdk_vdx6gx.dll
IMG platform version 305 loaded :)
Boards connected: (0,P4405C-00A#0306) (1,P4405C-00A#0310)
Board ID selected : 1
Initiating CCI communication at address 32
Sensor detected on interface 0
IMG_PLAT error (1): Error: Wait8, could not reach value 0 for register 513 last read: 1;(Failed to acknowledge command)

 

Still debugging, but going to but it up here in case someone has run into this before.

ST Employee
Jul 31, 2025 2:42 AM UTC

That is already a good progress as the two boards are well detected!

If you need further assistance for debugging, please provide your script so I can check it on my side.  

 

Best Regards,

 

Jean

oaa3wfAuthor
Associate II
Aug 4, 2025 7:52 PM UTC

Thanks @Jean_Poire , unfortunately, I wasn't able to figure out the issue. I notice that LED D6 goes red for a second when the problem occurs. I think it should be reproducible with the code below (and the SDK):

import os

from vdx6gx_constants import *
from vdx6gx_frame_decoding import decode_frame
from image_sensor_python_sdk import *
from smart_imshow import SmartImshow
import threading
import time

bits_per_pixel = BITS_8

x_start = 2
x_end = 1105
y_start = 2
y_end = 1361

# height = 640
# width = 480

# x_end = x_start + width - 1
# y_end = y_start + height - 1
width = x_end - x_start + 1
height = y_end - y_start + 1

data_rate_mbps = 1500

def getSensorDll(i2c_address: int = 32, boardId: int = 0):
 # Init the board
 sensor_dll = SensorDll(LIB_NAME, decode_frame)
 sensor_dll.init_board(i2c_address, board_id=boardId)
 sensor_dll.Write16(VDx6Gx_REG_STATICS_FORMAT_CTRL, bits_per_pixel)
 # Slave mode
 slave_mode = 2

 # Set the sensor configuration (VD55G1 specific)

 sensor_dll.Write16(VDx6Gx_REG_STATUS_FRAME_RATE, 30)
 sensor_dll.Write8(VDx6Gx_REG_STREAM_STATICS_ORIENTATION, 0)
 sensor_dll.Write16(VDx6Gx_REG_STREAM_CTX0_FRAME_LENGTH,4200)


 sensor_dll.Write16(VDx6Gx_REG_CONTEXTS_OUT_ROI_X_START, x_start)
 sensor_dll.Write16(VDx6Gx_REG_CONTEXTS_OUT_ROI_X_END, x_end)
 sensor_dll.Write16(VDx6Gx_REG_CONTEXTS_OUT_ROI_Y_START, y_start)
 sensor_dll.Write16(VDx6Gx_REG_CONTEXTS_OUT_ROI_Y_END, y_end)

 sensor_dll.reconfigure_csi_receiver(2, data_rate_mbps, 1116, 1356, bits_per_pixel, 160800000)
 # sensor_dll.reconfigure_csi_receiver(2, data_rate_mbps, 480, 642, bits_per_pixel, 160800000)
 sensor_dll.Write8(VDx6Gx_REG_STATUS_VT_CTRL, slave_mode)

 return sensor_dll




sensor_dll_0 = getSensorDll(32, 0)
sensor_dll_1 = getSensorDll(32, 1)
print("----------------------------------- done setting up", flush=True)

print("----------------------------------- starting streams", flush=True)
time.sleep(5.0)
sensor_dll_0.start_stream()
print("------started stream 0")
time.sleep(5.0)
sensor_dll_1.start_stream()
print("------started stream 1")

# sleep for 10 seconds and shutdown
time.sleep(10.0)

sensor_dll_0.stop_stream()
sensor_dll_1.stop_stream()
sensor_dll_0.deinit_board()
sensor_dll_1.deinit_board()



Thanks 

ST Employee
Aug 5, 2025 3:52 AM UTC

Hi @oaa3wf ,

There is indeed a small issue with the management of the dll. As you are trying to stream with 2 vdx6gx you are using the same dll. When you are initializing your second board you are overwriting the sensor_dll object and now both sensor_dll_0 and sensor_dll_1 are talking to the same board. That is why the second start_stream() raise an error as the sensor is already streaming. A workaround is to create a copy of the dll and make two call to two different dll: 

In my folder I have now 4 files :

st_brightsense_sdk_vdx6gx_0.dll

st_brightsense_sdk_vdx6gx_0.h

st_brightsense_sdk_vdx6gx_1.dll

st_brightsense_sdk_vdx6gx_1.h

Inside vdx6gx_constants.py:

SENSOR_DLL_NAME_0 = "st_brightsense_sdk_vdx6gx_0"
SENSOR_DLL_NAME_1 = "st_brightsense_sdk_vdx6gx_1"
LIB_NAME_0 = get_lib_name(SENSOR_DLL_NAME_0)
LIB_NAME_1 = get_lib_name(SENSOR_DLL_NAME_1)

Inside your script:

sensor_dll = SensorDll([LIB_NAME_0, LIB_NAME_1][boardId], decode_frame)

 I was able to make it work on my side using this workaround. I will search for the root cause and better solution when I have the bandwidth.

 

Sorry for the troubles,

Best regards,

Jean