Skip to main content
KHütt.1
Associate
July 21, 2020
Question

Whats about the long term stability VL53L1X? Can it work for 30 years 24/7?

Hi,

We're planning to use the sensor in an application with long live available.

Are there data available?

Regards,

Kilian

This topic has been closed for replies.

2 replies

John E KVAM
ST Employee
July 21, 2020

At the lowest level the Vertical Cavity Surface Emitting Laser (VCSEL) is an LED with mirrors. Techically it should last longer than an LED. These devices drive all the fiber-optic telecommunications in the world. The Single Photon Avalanche Diode (SPAD) array is similarly just a fancy bunch of diodes. Ok, a very fancy bunch, but the technology is well understood. The controller between them is one of the most widly deployed MCUs. That should not be a problem.

The silicon is not the issue. But this chip has an internal structure. The lens and the cap are attached with glue. In theory the glue should last forever, but with enough heating and cooling over 30 years it might fail.

We run a lot of industry standard tests on our part, and the statistics say it will run for thousands of years. But the truth is we got NO failures in all the accelarated testing we did, and statistics don't work well when you get no failures.

That being said, Temperature and over-voltage are the two things that can kill the sensor. Keep those in range and our testing says it should last for well over 30 years.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
KHütt.1
KHütt.1Author
Associate
July 22, 2020

Thank you John.

That sounds very good. So I'm not in worry about the sensor.

We'll test the sensor in our application with heating and cooling. If we have a fail I'll contact you again.