Skip to main content
SShah.20
Associate
April 12, 2022
Question

We are using VL53L3CX-SATEL in one of our applications. The problem we are facing is of mounting this small module. What possible options do we have to mount this small module. Any suggestion is well appreciated

  • April 12, 2022
  • 2 replies
  • 1167 views

..

This topic has been closed for replies.

2 replies

Julien NGUYEN
ST Employee
April 12, 2022

Hi,

Sorry, could you describe a little bit more the problem you are facing. Usually in the VL53L3CX-SATEL you have two parts offering two possible use-cases. The 1st use case could be that the VL53L3CX-SATEL is be mounted on an X-NUCLEO-53L3A2 board or you can only use the breakout part of the SATEL to connect to your electronic system thanks to some wires soldered on the breakout part.

Thanks,

Julien

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
John E KVAM
ST Employee
April 13, 2022

There is a company called Hornix.com.tw that mounts the sensors on little bits of circuit board and then sticks a coverglass on top. (got to hornix.com.tw and click on "Product" and scroll to almost the bottom.

Or you could use a flex and do the same thing.

But what a lot of people do is just sick the sensor on the PCB board and design the housing such that the coverglass is really close to the sensor.

  • john0693W00000Lxul0QAB.png
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.