Skip to main content
TCimi.1
Associate
April 13, 2023
Question

We are using VL53L0X ToF sensors. Our normal solder assembly process involves ultrasonically cleaning the PCB assembly in liquid. I gather that any kind of liquid immersion can harm the sensor. Is there a recommended way to remove flux residue?

  • April 13, 2023
  • 3 replies
  • 1253 views

..

This topic has been closed for replies.

3 replies

Zhiyuan.Han
ST Technical Moderator
April 18, 2023

Hi TCimi

​

Yes, you concern is totally correct, the liquid will damage the TOF sensor as it is not waterproof design.

To remove flux, my suggestion is you can clean the flux manually with cotton swab dip with flux cleaner.

if there are some dust/smudges on the PCB, you can use a powerful vacuum cleaner to remove them.

​

Br

Zhiyuan.Han​

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
TCimi.1
TCimi.1Author
Associate
April 20, 2023

Thank you, Zhiyuan.

I'm also worried about flux residue under the ToF sensor which could cause low-impedance between connections. Is there a certain type of solder paste you recommend?

Zhiyuan.Han
ST Technical Moderator
April 21, 2023

Hi TCimi

For PCB soldering process, actually you can treat TOF as normal device, just need pay attention to the peak temperature.

I suggest you contact with your PCB solder vendor for solder past question, sorry can't help on this question.

br

Zhiyuan.Han

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.