Skip to main content
Jacek Pieczaba
Associate III
December 11, 2023
Solved

VL6180 AVDD question

  • December 11, 2023
  • 2 replies
  • 1886 views

Hello,

I am planning to use VL6180 sensor in my application which is going to communicate with STM32L071. I would like to ask a question since the specification for the AVDD mentioning about optimal value is 2.8V. Do I need to provide some special LDO for stabilization this voltage (ripple reduction, etc.) or I can supply VL6180 directly from step down converter as long as I keep +/-100mV tolerance on 2.8V output? 

JacekPieczaba_1-1702313620102.png

STM32L071 should works well. 

Thank you in advance for your help and sorry if this question was already answered but I had difficulty to find it. 

Jacek 

This topic has been closed for replies.
Best answer by John E KVAM

The sensor does not depend on clean power. And an LDO is fine. As the sensor uses a digitally controlled Vertical Cavity Surface Emiting Laser (VCSEL) and does NOT depend on amount of signal return, your power does NOT have to be spot on. 

- john

2 replies

John E KVAM
John E KVAMBest answer
ST Employee
December 11, 2023

The sensor does not depend on clean power. And an LDO is fine. As the sensor uses a digitally controlled Vertical Cavity Surface Emiting Laser (VCSEL) and does NOT depend on amount of signal return, your power does NOT have to be spot on. 

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Jacek Pieczaba
Associate III
December 17, 2023

Thank you very much

- Jacek