Skip to main content
Associate II
August 11, 2026
Question

VL53L9CX precision and accuracy

Hello, 

I am using VL53L9CX with adapted drivers for ESP32 / Arduino environment. 

I am able to read values and play with the settings but I am a bit worried with the precision I get. 

I run the sensor in precision mode, 4ms exposure time. My bench is indoor. Sensor facing the ground ( 1 m ish, wood) or the roof (1.6m ish, white ceiling). Resolution is 8 x 6 (Binning 12). 
I have radial to perpendicular conversion enabled so I am expecting to see all distances being equal +/- precision across the cells of the frame (excluding corner cells maybe). 

According to table 34: Precision for “ambient mode 24x20” profile from the sensor datasheet: (results are better for 24*20 then they are for 54*42, so I assume it is the same or better for 8*6 compared to 24*20)
I am expecting less than 0.8 mm difference between the values but instead I get 50 mm - 100 mm or more of difference. 
So I was wondering, is there some specific settings to enable to achieve such precision / accuracy ? 

PCB is of my own (not an evaluation board). Sensor is facing ground / roof within a few degrees of roll/pitch as I place it manually but nothing that would explain such delta in between the values after radial to perpendicular conversion. 

I would appreciate any guidance. 
I can share further details if you need anything.

Thanks
Thomas

3 replies

Visitor
September 6, 2026

Where i can get this board?

If possible can i get your designed gerber file pls.

Peter BENSCH
ST Technical Moderator
September 6, 2026

​@rau7han please see my answer in your other thread.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MeganeG
ST Technical Moderator
September 28, 2026

Hello ​@thomasboutant,

High binning will improve the SNR, and you will have a stronger signal. It is therefore possible that the sensor is saturating. Have you tried reducing the exposure time to see if you have better results?

Thanks, Megane

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.