Skip to main content
Senior
June 27, 2024
Question

Vl53L8CX with STM32WB5mm-DK

  • June 27, 2024
  • 1 reply
  • 629 views

I am using Vl53l8cx with stm32wb5mmdk.  I am unable to initialize the sensor via this board. I used  it with a nucleo board and it worked fine, but I need a BLE-based controller to share data.

SDA  and SCL are pulled up with 4.7k 3v3 is connected to 5vo via voltage divider giving 3.3 volts , 1v8 is connected to 5VO via voltage divide giving 1.8 volts. SPI_I2c_N is connected to gnd pin.

All other connections are in the project file itself.

The link below will take you to the project file 

Project 

This topic has been closed for replies.

1 reply

RiturajAuthor
Senior
July 1, 2024

I have tried all I could but have not been able to find the issue. I have configured LPUART instead of USART for trace related to BLE . Can this be a possible reason .

 

I need immediate help with this . It would be great if someone could give me even an idea of how it needs to be don.