Skip to main content
Visitor II
Sep 19, 2024 9:55 AM UTC
Solved

VL53l8CX SPI not working

Hi,

I am using VL53L8CX sensor from Pololu and connected it with Nucleo-F411RE board. I am using Arduino IDE 2.3 where I have downloaded STM32duino VL53L8CX library. When I run HelloWorld_I2C example with the wire  connections as mentioned with (SPI/I2c-->GND, Lpn-->A3), I am getting the distance result. But when I do the same with the HelloWorld_SPI example with mentioned connection (SPI/I2c-->3v3, Lpn-->3v3), I am getting nothing. When I put the breaker in between, the initialization itself fails saying sensor initialization status 1. 

I would be a great relief if you could help me with this.

Thank you

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
Sep 23, 2024 10:45 PM UTC

This problem is the same as:

 
Basically, the manufacturer thought he would save some money and switched a part on the board. 
- john
 
 
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

2 replies

John E KVAM
John E KVAMBest answer
ST Employee
Sep 23, 2024 10:45 PM UTC

This problem is the same as:

 
Basically, the manufacturer thought he would save some money and switched a part on the board. 
- john
 
 
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
256
Associate
Feb 4, 2025 4:42 PM UTC

I am having the same problem here, but I know that I have the correct chips on my board (at least, the level shifters are labeled that they are both PI4ULS3V204s). After set up, it seems that the VL53L8CX's status is 0, but any calls to communicate with the sensor are left hanging, and no response is ever recieved. If anyone has SPI working with their VL53L8CX, could you share your pin assignments with me?