Skip to main content
MCham.8
Visitor II
June 7, 2023
Question

VL53L8CX SATEL use with Arduino Or ESP32?

Does anyone know if the VL53L8CX SATEL can be used with an Arduino board (just for testing)? Or ESP32? I've tried the basic wiring I have done for other breakouts, but it doesn't work.

 

If so, please share how it should be wired. Also, I have used very similar code on 1CB, 1CX, and the 4CX. Anyone know if that would work for the L8?

This topic has been closed for replies.

5 replies

John E KVAM
ST Employee
June 7, 2023

The VL53L5, L7 and L8 are multi-zone sensors. Instead of getting 1 distance per range, you get 64 of them. And if you want signal strengths, multiple targets per zone and other information you can get some like 6000 bytes of return data every 15th of a second. It's a lot.

And it does download the firmware into the sensor at startup. That's some 83Kbytes.

This is getting pretty large for a little processor.

But it can be done.

you need to have the I2C select pin grounded, and the LPn pin raised. You need power and I2C. Interrupt is helpful - but not required.

The easy way is to wait. Sparkfun is soon to release just what you want.

This sensor works the same way is all our other VL53 products. It's your job to complete the platform.c for your processor. This file is the interface to the MCU's I2C. As delivered it's empty. But if you've already done the L1 or L4, it should be easy to adapt.

So providing your MCU is big enough, it will work.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Associate
May 14, 2024

And what about his SPI interface ?

thx

Associate
July 15, 2024

Equally confused about this. There seems to be plenty of configuration support for the I2C interface, but I have yet to find anything that supports the SPI interface.