Skip to main content
Visitor II
December 31, 2024
Solved

VL53L8CX Platform Integration with ChibiOS

Hi, I am trying to integrate the VL53L8CX ULD driver with a project that utilizes chibios on an F4 based board.
The TOF sensor firmware seems to be about 86KB. For a transfer of this size, the device fails to setup and use DMA-safe bouncebuffers. I cannot get it to transfer more than 9865 bytes at once. Can the VL53L8CX_WrMulti(...) calls be broken down into smaller chunks as a work around? If I understand correctly, this is using the auto increment feature of the I2C bus. So to further break the VL53L8CX_WrMulti(...) calls, I will have to ensure the address for each call is sent appropriately. So will this work?
//in vl53l8cx_init(...)
status |= VL53L8CX_WrMulti(&(p_dev->platform),0,(uint8_t*)&VL53L8CX_FIRMWARE[0],0x2000);
status |= VL53L8CX_WrMulti(&(p_dev->platform),0x2000,(uint8_t*)&VL53L8CX_FIRMWARE[0x2000],0x2000);
status |= VL53L8CX_WrMulti(&(p_dev->platform),0x4000,(uint8_t*)&VL53L8CX_FIRMWARE[0x4000],0x2000);
status |= VL53L8CX_WrMulti(&(p_dev->platform),0x6000,(uint8_t*)&VL53L8CX_FIRMWARE[0x6000],0x2000);

Instead of
status |= VL53L8CX_WrMulti(&(p_dev->platform),0,(uint8_t*)&VL53L8CX_FIRMWARE[0],0x8000);

Also, what is the purpose of the register with address 0x7fff?

TIA

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
January 2, 2025

That is exactly what you have to do if you cannot write a huge I2C transaction in one go. 

And the 0x7fff is a page register. Unless it's the last write of a long transaction in which case it a 'go' command. 

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

1 reply

John E KVAM
John E KVAMBest answer
ST Employee
January 2, 2025

That is exactly what you have to do if you cannot write a huge I2C transaction in one go. 

And the 0x7fff is a page register. Unless it's the last write of a long transaction in which case it a 'go' command. 

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.