Skip to main content
Associate II
Dec 12, 2024 11:46 PM UTC
Solved

Vl53l8 configuring the ranging frequency

Hi,

I am using the VL53l8 sensor. i need to change the ranging frequency. im using the Xcube tof code. I see in the app tof code that #define RANGING_FREQUENCY (10U). so if i change 10u to 15. Willi get ranging frequency to 15 hz.?

 

Thank u 

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
Dec 13, 2024 5:59 PM UTC

that should work just fine. 

and, as you are using an STM32, go ahead and insert:

//Counting cycles is a piece of cake. 
//Stick this code somewhere in your code.

 cur_timestamp = HAL_GetTick();
 printf("%4lums \n",cur_timestamp - prev_timestamp);
 prev_timestamp = cur_timestamp;

Each tick is a ms. - but remember that there is going to be a roll-over at some point. But it's great for just testing!!

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

1 reply

John E KVAM
John E KVAMBest answer
ST Employee
Dec 13, 2024 5:59 PM UTC

that should work just fine. 

and, as you are using an STM32, go ahead and insert:

//Counting cycles is a piece of cake. 
//Stick this code somewhere in your code.

 cur_timestamp = HAL_GetTick();
 printf("%4lums \n",cur_timestamp - prev_timestamp);
 prev_timestamp = cur_timestamp;

Each tick is a ms. - but remember that there is going to be a roll-over at some point. But it's great for just testing!!

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.