Skip to main content
Associate II
April 8, 2024
Solved

VL53L7X get Point Cloud

Hi, I'm trying to create a 4x4 point cloud using a VL53L7CX-Sensor. I already got the x, y and z, but I am not sure if the values are right. My approach:

*iter_x = static_cast<float>(kMillimeterToMeter * cos(w * fovPerPixel - kFov / 2.0f - DegToRad(90.0f)) * depth);
*iter_y = static_cast<float>(kMillimeterToMeter * sin(h * fovPerPixel - kFov / 2.0f) * depth);
*iter_z = static_cast<float>(kMillimeterToMeter * depth);

Hartm_Sve_0-1712560687133.png

But the points doesn't seem right...

Any help would be appreciated!

 

 

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
April 8, 2024

It's been posted before. 

VL53L5CX Multi-Zone Sensor get x,y,z of points rel... - STMicroelectronics Community

the L5 and the L8 have the same FoV. So that code is the same.

The L7 has a 60x60 FoV so that code is the same but with different angles.

- john

 

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

9 replies

John E KVAM
John E KVAMBest answer
ST Employee
April 8, 2024

It's been posted before. 

VL53L5CX Multi-Zone Sensor get x,y,z of points rel... - STMicroelectronics Community

the L5 and the L8 have the same FoV. So that code is the same.

The L7 has a 60x60 FoV so that code is the same but with different angles.

- john

 

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Hartm_SveAuthor
Associate II
April 11, 2024

How do you get the values of Pitch and Yaw?

ST Employee
April 11, 2024

Roughly the FoV of each zone in the L5, L7 and L8 devices are as follows:
VL53L5 = 5.25 degrees
VL53L7 = 7.5 degrees
VL53L8 = 5.25 degrees

You can see the 5.25 degrees here matches the values used in the code that John referenced for the L5 part. 
Roger

Roger SHIVELY
ST Employee
April 15, 2024

Hey @Hartm_Sve 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Roger

Hartm_SveAuthor
Associate II
July 23, 2024

Hi, i know this topic has been closed for months. But I am trying to reduce my cycle time and i would appreciate if you could send me the Pitch and Yaw for a VL53L7CX.

Thanks!

 

John E KVAM
ST Employee
July 23, 2024

Follow the link in the accepted solution above and you will get to the following table. 

VL53L5CX Multi-Zone Sensor get x,y,z of points rel... - STMicroelectronics Community

It also has code.

#ifdef VL53L5
const double VL53L5_Zone_Pitch8x8[64] = {
		59.00,64.00,67.50,70.00,70.00,67.50,64.00,59.00,
		64.00,70.00,72.90,74.90,74.90,72.90,70.00,64.00,
		67.50,72.90,77.40,80.50,80.50,77.40,72.90,67.50,
		70.00,74.90,80.50,85.75,85.75,80.50,74.90,70.00,
		70.00,74.90,80.50,85.75,85.75,80.50,74.90,70.00,
		67.50,72.90,77.40,80.50,80.50,77.40,72.90,67.50,
		64.00,70.00,72.90,74.90,74.90,72.90,70.00,64.00,
		59.00,64.00,67.50,70.00,70.00,67.50,64.00,59.00
};
#else	//VL53L7
const double VL53L5_Zone_Pitch8x8[64] = {
		52.00,56.00,61.00,64.00,64.00,61.00,56.00,52.00,
		56.00,62.00,67.00,70.00,70.00,67.00,62.00,56.00,
		61.00,67.00,76.00,78.00,78.00,76.00,67.00,61.00,
		64.00,70.00,78.00,84.00,84.00,78.00,70.00,64.00,
		64.00,70.00,78.00,84.00,84.00,78.00,70.00,64.00,
		61.00,67.00,76.00,78.00,78.00,76.00,67.00,61.00,
		56.00,62.00,67.00,70.00,70.00,67.00,62.00,56.00,
		52.00,56.00,61.00,64.00,64.00,61.00,56.00,52.00
};
#endif  

 

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.