Skip to main content
KNawa.1
Associate II
April 12, 2023
Question

VL53L5CX/VL53L7CX - material type recognition

In "Enhance Time-of-Flight

performance with new sensors based on the world’s first optical metasurface

technology " webinar it was presented simple way of material

recognition of floor type for vacuum cleaner. could you tell me which parameter

from "VL53L5CX_ResultsData" structure was used to support this?

to be more precise structure as below:

"typedef struct

{

/* Internal sensor silicon temperature */

int8_t silicon_temp_degc;

/* Ambient noise in kcps/spads */

#ifndef VL53L5CX_DISABLE_AMBIENT_PER_SPAD

uint32_t ambient_per_spad[VL53L5CX_RESOLUTION_8X8];

#endif

/* Number of valid target detected for 1 zone */

#ifndef VL53L5CX_DISABLE_NB_TARGET_DETECTED

uint8_t nb_target_detected[VL53L5CX_RESOLUTION_8X8];

#endif

/* Number of spads enabled for this ranging */

#ifndef VL53L5CX_DISABLE_NB_SPADS_ENABLED

uint32_t nb_spads_enabled[VL53L5CX_RESOLUTION_8X8];

#endif

/* Signal returned to the sensor in kcps/spads */

#ifndef VL53L5CX_DISABLE_SIGNAL_PER_SPAD

uint32_t signal_per_spad[(VL53L5CX_RESOLUTION_8X8

*VL53L5CX_NB_TARGET_PER_ZONE)];

#endif

/* Sigma of the current distance in mm */

#ifndef VL53L5CX_DISABLE_RANGE_SIGMA_MM

uint16_t range_sigma_mm[(VL53L5CX_RESOLUTION_8X8

*VL53L5CX_NB_TARGET_PER_ZONE)];

#endif

/* Measured distance in mm */

#ifndef VL53L5CX_DISABLE_DISTANCE_MM

int16_t distance_mm[(VL53L5CX_RESOLUTION_8X8

*VL53L5CX_NB_TARGET_PER_ZONE)];

#endif

/* Estimated reflectance in percent */

#ifndef VL53L5CX_DISABLE_REFLECTANCE_PERCENT

uint8_t reflectance[(VL53L5CX_RESOLUTION_8X8

*VL53L5CX_NB_TARGET_PER_ZONE)];

#endif

/* Status indicating the measurement validity (5 & 9 means ranging OK)*/

#ifndef VL53L5CX_DISABLE_TARGET_STATUS

uint8_t target_status[(VL53L5CX_RESOLUTION_8X8

*VL53L5CX_NB_TARGET_PER_ZONE)];

#endif

/* Motion detector results */

#ifndef VL53L5CX_DISABLE_MOTION_INDICATOR

struct

{

uint32_t global_indicator_1;

uint32_t global_indicator_2;

uint8_t status;

uint8_t nb_of_detected_aggregates;

uint8_t nb_of_aggregates;

uint8_t spare;

uint32_t motion[32];

} motion_indicator;

#endif

} VL53L5CX_ResultsData;

" 

This topic has been closed for replies.

1 reply

KNawa.1
KNawa.1Author
Associate II
April 14, 2023

just for Others: based on my check "reflectance" depends on material type, others not.