Skip to main content
AlexCloned
Senior
April 1, 2022
Solved

VL53L5CX ULD. Is Timing Budget equal to Integration time for Autonomous ranging mode?

When filling the struct in my app

typedef struct
{
 uint32_t RangingProfile;
 uint32_t TimingBudget; /*!< Expressed in milliseconds */
 uint32_t Frequency; /*!< Expressed in Hz */
 uint32_t EnableAmbient; /*!< Enable: 1, Disable: 0 */
 uint32_t EnableSignal; /*!< Enable: 1, Disable: 0 */
} RANGING_SENSOR_ProfileConfig_t;

I am a bit confused about the TimingBudget in it.

I followed function calls starting in the nucleo examples at

VL53L5A1_RANGING_SENSOR_ConfigProfile(i, &Profile);

And this ends up assigning the TimingBudget into a variable named integration_time !

integration_time = pConfig->TimingBudget;

later I miss the footprints of this integration_time when the api sends its value to a memory_buffer with the function "vl53l5cx_dci_replace_data".

Can you confirm this integration_time is the one used in autonomous ranging mode?

Then, in continuous mode, if I want to increase the timing budget I must just set up the proper ranging frequency, disregarding the Timing Budget value set in the RANGING_SENSOR_ProfileConfig_t struct. Right?

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
April 4, 2022

There are 2 ways you can do this. Tiimed mode, and Back-to-Back. If you are doing B2B, then choosing a TimingBudget will give you the frequency of the results. The sensor will consume all the time allocated to it and provide the answers

But if you want a 'quiet' period between the ranges, then you choose a ranging frequency. Let's say 1 range per second. And to save power, you can choose an integration time of 1/15 of a second. That way, 14/15 of the time, the sensor is just hanging around waiting for it's next time to run.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

1 reply

John E KVAM
John E KVAMBest answer
ST Employee
April 4, 2022

There are 2 ways you can do this. Tiimed mode, and Back-to-Back. If you are doing B2B, then choosing a TimingBudget will give you the frequency of the results. The sensor will consume all the time allocated to it and provide the answers

But if you want a 'quiet' period between the ranges, then you choose a ranging frequency. Let's say 1 range per second. And to save power, you can choose an integration time of 1/15 of a second. That way, 14/15 of the time, the sensor is just hanging around waiting for it's next time to run.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.