Skip to main content
Explorer
January 23, 2025
Question

VL53L5CX platform code using Raspberry Pi Pico

Hi there,

I'm currently trying to write the platform code for the VL53L5CX using a Raspberry Pi Pico.

I'm trying to publish the sensor data via micro-ROS in a ROS2 topic. When I use my current code I only get values close to zero and they are the same every time so I think the problem is in the I2C connection. I used an I2C-Scan so I know that the address is 0x29.

The only thing I could find online that was close to a platform code using a Pico was the platform code for a VL53L1X. Could anybody tell what I did wrong or how I have to configure the platform code for the VL53L1X so I can use it with the VL53L5CX.

Thanks a lot :)

Current platform.c:

 

/**
 *
 * Copyright (c) 2021 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */

#include "hardware/i2c.h"
#include <stdbool.h>
#include "platform.h"

uint8_t VL53L5CX_WrByte(
 VL53L5CX_Platform *p_platform,
 uint16_t RegisterAdress,
 uint8_t value)
{
 uint8_t buffer[3];
 buffer[0] = (RegisterAdress >> ‌8)‌ & 0xFF;
 buffer[1] = RegisterAdress & 0xFF;
 buffer[2] = value;

 p_platform->address = 0x29;

 int result = i2c_write_blocking(i2c0, p_platform->address, buffer, sizeof(buffer), false);
 return (result < 0) ? 1 : 0;
}


uint8_t VL53L5CX_RdByte(
 VL53L5CX_Platform *p_platform,
 uint16_t RegisterAdress,
 uint8_t *p_value)
{
 uint8_t buffer[2];
 buffer[0] = (RegisterAdress >> ‌8)‌ & 0xFF; // High-Byte der Registeradresse
 buffer[1] = RegisterAdress & 0xFF; // Low-Byte der Registeradresse

 p_platform->address = 0x29;

 // Registeradresse senden
 int result = i2c_write_blocking(i2c0, p_platform->address, buffer, sizeof(buffer), true);
 if (result < 0)
 {
 return 1; // Fehler
 }

 // Byte lesen
 result = i2c_read_blocking(i2c0, p_platform->address, p_value, 1, false);
 return (result < 0) ? 1 : 0; // 0 = Erfolg, 1 = Fehler
}


uint8_t VL53L5CX_WrMulti(
 VL53L5CX_Platform *p_platform,
 uint16_t RegisterAdress,
 uint8_t *p_values,
 uint32_t size)
{
 p_platform->address = 0x29;

 uint8_t buffer[2 + size];
 buffer[0] = (RegisterAdress >> ‌8)‌ & 0xFF; // High-Byte der Registeradresse
 buffer[1] = RegisterAdress & 0xFF; // Low-Byte der Registeradresse
 memcpy(&buffer[2], p_values, size); // Daten kopieren

 int result = i2c_write_blocking(i2c0, p_platform->address, buffer, sizeof(buffer), false);
 return (result < 0) ? 1 : 0; // 0 = Erfolg, 1 = Fehler
}


uint8_t VL53L5CX_RdMulti(
 VL53L5CX_Platform *p_platform,
 uint16_t RegisterAdress,
 uint8_t *p_values,
 uint32_t size)
{
 p_platform->address = 0x29;

 uint8_t buffer[2];
 buffer[0] = (RegisterAdress >> ‌8)‌ & 0xFF; // High-Byte der Registeradresse
 buffer[1] = RegisterAdress & 0xFF; // Low-Byte der Registeradresse

 // Registeradresse senden
 int result = i2c_write_blocking(i2c0, p_platform->address, buffer, sizeof(buffer), true);
 if (result < 0)
 {
 return 1; // Fehler
 }

 // Daten lesen
 result = i2c_read_blocking(i2c0, p_platform->address, p_values, size, false);
 return (result < 0) ? 1 : 0; // 0 = Erfolg, 1 = Fehler
}

uint8_t VL53L5CX_Reset_Sensor(
		VL53L5CX_Platform *p_platform)
{
	uint8_t status = 0;
	
	/* (Optional) Need to be implemented by customer. This function returns 0 if OK */
	
	/* Set pin LPN to LOW */
	/* Set pin AVDD to LOW */
	/* Set pin VDDIO to LOW */
	VL53L5CX_WaitMs(p_platform, 100);

	/* Set pin LPN of to HIGH */
	/* Set pin AVDD of to HIGH */
	/* Set pin VDDIO of to HIGH */
	VL53L5CX_WaitMs(p_platform, 100);

	return status;
}

void VL53L5CX_SwapBuffer(
		uint8_t 		*buffer,
		uint16_t 	 	 size)
{
	uint32_t i, tmp;
	
	/* Example of possible implementation using <string.h> */
	for(i = 0; i < size; i = i + 4) 
	{
		tmp = (
		 buffer[i]<<24)
		|(buffer[i+1]<<16)
		|(buffer[i+2]<<8)
		|(buffer[i+3]);
		
		memcpy(&(buffer[i]), &tmp, 4);
	}
}	

uint8_t VL53L5CX_WaitMs(
		VL53L5CX_Platform *p_platform,
		uint32_t TimeMs)
{
	uint8_t status = 255;

	/* Need to be implemented by customer. This function returns 0 if OK */
	
	return status;
}

 

 

 

 

 

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
January 23, 2025

A couple of comments:

Check Gethub. The linux community is good at sharing code. I found GitHub - akionu/pico-vl53l5cx: A Tiny Library for ST's VL53L5CX using Raspberry Pi Pico C/C++ SDK 

which looks very promising. 

 In my experience the i2c issues generally boil down to byte-swap (and word-swap) issues. 

Sometimes I see a set-up with long wires, and that can cause electrical issues. But if you aren't getting anywhere at the start, it's a byte-swap issue.

Checkout the github, and see what they did. That should get you going. 

- john 

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.