Skip to main content
Associate
September 16, 2024
Solved

VL53L5CX Outlier values and Fluctuations

  • September 16, 2024
  • 3 replies
  • 2081 views

Firstly, on behalf of our company, I would like to appreciate the great products that have been delivered by STM through the years, wish STM well and prosper.

#----------------------------------------------------------------------------------------------------

Recently we are working on using the VL53L5CX TOF for our ML project.

Settings in fw :

I2C speed : 1MHz

Resolution : 8x8

Ranging Frequency : 2Hz

Ranging Mode : Continuous

Target Order : Closest

Sharpener Percentage : 20%

MCU : ESP-32

Platform : Arduino IDE

With Cover Glass

Room environment, curtains are opened

Embedded_William_6-1726520754456.png

Graphing software : Processing Grapher

 

Constraints :

- Sensor will be installed on ceiling, facing the ground, around a distance of 2.5m to 3m

- Must use all 8x8 SPAD sensors

- Sharpener value should be around 20%, since we are planning to use all the SPAD, as the sharpener increases, edge values readings become vague

Embedded_William_3-1726520397814.png

 

#----------------------------------------------------------------------------------------------------

Case 1 : Facing the ceiling, steady

Embedded_William_7-1726520786150.png

Observation : Takes some time for the outlier values to return to normal value

Embedded_William_0-1726519721337.png

 

Case 2 : Waved my hand once above the TOF

Observation : Some outlier values appear (purple blue around 0mm) after my hand are no longer on the TOF

Embedded_William_1-1726519742941.png

 

Case 3 : With my hands 20cm on top of the TOF, steady

Observation : Values are fluctuating

Embedded_William_2-1726519803919.png

 

Case 4 : TOF facing the pillows, steady

Embedded_William_5-1726520724279.png

Observation :

Embedded_William_8-1726520867154.png

We have also tried to have the TOF installed on the ceiling and facing the chairs & table etc, but the output are fluctuating as well.

#----------------------------------------------------------------------------------------------------

For Case 1 & 2, why do the outlier values take a long time to return to the normal reading position?

-> How do we have those outlier value returned to the normal position quick?

 

Our doubt is that, with case 3 & 4, since everything in the scenario is steady (not moving).
->Why is the output of the values fluctuating?

 

Our understanding to the sensor is that, if the TOF is facing/ sensing an area with non-moving/steady objects, it should return stable values, and values should not be fluctuating. Is it related to the settings in the fw?

We have tried to calibrate the sensors with the proposed setting by STM, i.e :

Embedded_William_9-1726523511657.png

Also tried with and without the cover glass, but the fluctuation persists.

Stable values would be really helpful for building the ML model when collecting the data.

 

We look forward to the discussion. Thank you.

Cheers

Will

 

This topic has been closed for replies.
Best answer by John E KVAM

No. In autonomous mode you integrate for maybe 10ms then go to sleep for a 490ms then range again for 10ms. That way you get 2 measures per second but don't spend the power.

Continuous ranging means integrating until its time to start another range. Probably not what you want. 

In all cases the L8 is a better sensor. Shift to it if you can. 

There are 64 zones and in theory each zone can return 4 targets. But in practice two targets is kind of the practical limit. 

If you look down on a bed, some zones will see the bed, some will see the floor. Some zones will see both the bed and the floor. 

I generally sort by closest. In most cases closest is strongest as near targets return more photons than do far ones. 

But say your floor were particularly reflective and the bedding was not. Possible to have the floor be stronger. 

If you go through the structure (and you configure your platform.h to specify 2 targets) you will see them in each of the 64 zones.

- john 

3 replies

John E KVAM
ST Employee
September 16, 2024

Number 1 - go immediately to the VL53L8. Same price, Same FoV, better performance. (We improved the optical elements - but also changed a lot of other things as well.)

The fluctuations are due to the fact that under the covers we do 4, 4x4 sub ranges and stitch them together.  And with fast movement the 4 sub-ranges don't line up. 

Number 2 - Doing 2Hz continuous, means you are integrating for a full 1/2 second. 

Don't do this. 

Instead change the mode to Autonomous and integrate for something reasonable. 10ms is more than enough.

You might even like 5ms better. Try this even before going to the L8.

I recommend both of these, but just try #2 and see if it solves your issues.

- john

 

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Associate
September 17, 2024

Thank you for the reply John.
We did tried different frequencies from 2 - 15. But seems the fluctuations persists.
We chose 2Hz because of a slower retrieve rate, the fluctuations would be reduced since value changes less frequently. (But still fluctuates)

#----------------------------------------------------------------------------------------------------

Regarding the 10ms and 5ms you recommended, do you mean :

10Hz and 5Hz?

Period : 10ms = 0.01s, frequency is 100Hz, but seems it is not correct because 15Hz is the max freq. for 8x8

 

However I have changed the fw setting to what you recommended : Autonomous mode and 10Hz (I assume).

Read for 10 seconds, the sensor is placed steadily and is facing the ceiling, no moving objects is in the FOV.

Embedded_William_1-1726531777677.png

-> Seems there are lots of fluctuations going on

#----------------------------------------------------------------------------------------------------

Other than that, regarding the target order, how does one choose the best ?
Since all the 8x8 values are retrieved from the [1,1] to [8,8] (assume the SPAD to be a 8x8 matrix), how does the target order affect these values?

Embedded_William_0-1726531261341.png

#----------------------------------------------------------------------------------------------------

Lastly, regarding the VL53L8, would it give more stable values, and less outlier values? Thank you.

The sensor will be used on ceiling and facing the floor, no direct sunlight shining at the sensor.

 

Cheers

Will

John E KVAM
John E KVAMBest answer
ST Employee
September 17, 2024

No. In autonomous mode you integrate for maybe 10ms then go to sleep for a 490ms then range again for 10ms. That way you get 2 measures per second but don't spend the power.

Continuous ranging means integrating until its time to start another range. Probably not what you want. 

In all cases the L8 is a better sensor. Shift to it if you can. 

There are 64 zones and in theory each zone can return 4 targets. But in practice two targets is kind of the practical limit. 

If you look down on a bed, some zones will see the bed, some will see the floor. Some zones will see both the bed and the floor. 

I generally sort by closest. In most cases closest is strongest as near targets return more photons than do far ones. 

But say your floor were particularly reflective and the bedding was not. Possible to have the floor be stronger. 

If you go through the structure (and you configure your platform.h to specify 2 targets) you will see them in each of the 64 zones.

- john 

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.