Skip to main content
MFabb.1
Associate III
February 17, 2023
Solved

VL53L5CX Offset Calibration

Hi,

I noticed that an offset calibration function is missing in the API of the VL53L5CX (like seen before on VL53L1CX). Only the xtalk calibration is available.

Is this because all the VL53L5CXs are individually factory offset-calibrated?

My assumption is also based on the following section of the vl53l5cx_init() function:

	/* Get offset NVM data and store them into the offset buffer */
	status |= WrMulti(&(p_dev->platform), 0x2fd8,
		(uint8_t*)VL53L5CX_GET_NVM_CMD, sizeof(VL53L5CX_GET_NVM_CMD));
	status |= _vl53l5cx_poll_for_answer(p_dev, 4, 0,
		VL53L5CX_UI_CMD_STATUS, 0xff, 2);
	status |= RdMulti(&(p_dev->platform), VL53L5CX_UI_CMD_START,
		p_dev->temp_buffer, VL53L5CX_NVM_DATA_SIZE);
	(void)memcpy(p_dev->offset_data, p_dev->temp_buffer,
		VL53L5CX_OFFSET_BUFFER_SIZE);
	status |= _vl53l5cx_send_offset_data(p_dev, VL53L5CX_RESOLUTION_4X4);

where offset data are readed from NVM and loaded into the offset buffer.

Offset calibration on host side must be implemented when VL53L5CX is integrated behind a clear plastic glass with low crosstalk component?

Thank you

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
February 17, 2023

Actually we do an offset calibration on all our parts. But it was seen that the offset changed on a lot of the single-zone parts after the parts were soldered onto boards. The solution was to recommend the offset calibration on the single zone parts.

But the multizone parts work differently. The factory calibration is holding up even after several reflow operations.

We are very pleased to be able to delete the offset calibration requirement.

And thanks for asking.

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

2 replies

John E KVAM
John E KVAMBest answer
ST Employee
February 17, 2023

Actually we do an offset calibration on all our parts. But it was seen that the offset changed on a lot of the single-zone parts after the parts were soldered onto boards. The solution was to recommend the offset calibration on the single zone parts.

But the multizone parts work differently. The factory calibration is holding up even after several reflow operations.

We are very pleased to be able to delete the offset calibration requirement.

And thanks for asking.

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
MFabb.1
MFabb.1Author
Associate III
February 17, 2023

Thank you John!

This should be reported somewhere in the datasheet or in a specific application note.