Skip to main content
DM.16
Visitor II
April 28, 2023
Question

VL53L4CX_SetUserROI purpose

I read that we can not set spad array size on VL53L4CX chip. What is the purpose of function VL53L4CX_SetUserROI, found in VL53L4CX driver?

I tried setting two zones or two user rois but detection doesn’t change.

Damjan

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
April 28, 2023

Damjan -

That function does work - as it limits the number of SPADS in the SPAD array. (There are 16x16 in the array. And you lower that number. But more than likely it will have no effect on the L4 sensors.

Without the lens of the VL53L1, any light that comes in will be captured by a random SPAD. The lens focuses right or left, up or down.

If you had a very short distance application then you could use this to prevent wild swings of SPAD settings as the sensor tried to adjust to your target. Needing to do is is very rare.

We considered removing it, but one customer wanted it and we felt it wasn't hurting anything.\

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.