Skip to main content
Visitor II
October 25, 2023
Solved

VL53L4CX not NewDataReady

  • October 25, 2023
  • 2 replies
  • 1802 views

Hello, i've been using a couple of VL53L4CX tof for a month with no problem so far, but recently i bought a few more and none of these work. (These new ones are the same model that the ones that worked).

Analyzing with a digital osciloscope the I2C commands i saw a difference between this two.

Apparently the two tofs seems to be sending without a problem the init commands, but when it tries to access this register (VL53LX_GPIO__TIO_HV_STATUS 0x0031), the one that works answers with a 0x02, meanwhile the bad one responds with a 0x03 (I attached both screenshots).

This happens in the driver's function VL53LX_GetMeasurementDataReady, when it calls VL53LX_is_new_data_ready in vl53lx_wait.c (I attached also a screenshot of this function)

 

Does anyone know why is this happening? Could it be solved by software? Or it's a hardware issue?

 

This topic has been closed for replies.
Best answer by John E KVAM

If you don't have a photo diode handy, check the laser is on using a webcam. Phone cameras don't always work for this. As some of them emitt 940nm light they have really good IR filters on them. 

Did you check the status on all the I2C initialization commands? Sometimes - due to long wires - the I2C bus does not communicate correctly and you get a mess. 

But I agree with Anne. Seems hardware related. Unless you changed some code.

2 replies

Anne BIGOT
ST Technical Moderator
November 14, 2023

Hello,
It seems to be more a HW issue than a SW one. Are you able to use a photo diode to check that the laser is on ?

Anne

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'
John E KVAM
John E KVAMBest answer
ST Employee
November 14, 2023

If you don't have a photo diode handy, check the laser is on using a webcam. Phone cameras don't always work for this. As some of them emitt 940nm light they have really good IR filters on them. 

Did you check the status on all the I2C initialization commands? Sometimes - due to long wires - the I2C bus does not communicate correctly and you get a mess. 

But I agree with Anne. Seems hardware related. Unless you changed some code.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.