VL53L4CX Histogram Data Interpreting
- 2 replies
- 1463 views
Hi! I've been testing the VL53L4CX sensor for the past few months and have finally decided to take a look at its additional histogram data. My most recent test is a measurement of an empty black bucket with a white sheet inside (to increase reflectivity). While the distance measured is accurate, the histogram data, which I expected to be somewhat static, seems to oscillate between two histogram shapes.
The data below is distance, minimum distance and max distance measured.
244,244,246, 2025-03-10 11:48:04.530766
241,241,330, 2025-03-10 11:48:04.727428
243,243,245, 2025-03-10 11:48:04.926467
241,241,330, 2025-03-10 11:48:05.124474
243,243,245, 2025-03-10 11:48:05.322733
241,241,330, 2025-03-10 11:48:05.519547
243,243,331, 2025-03-10 11:48:05.711350
Below are the histograms (AdditionalData.VL53LX_p_006.bin_data) for each measurement.
847,860,895,867,757,815,139036,190843,89753,1021,794,804,848,803,827,828,790,853,892,731,833,759,843,803, 2025-03-10 11:48:04.530766
704,729,118073,161246,72683,950,692,668,696,728,727,765,671,715,716,707,730,684,700,686,729,694,690,660, 2025-03-10 11:48:04.727428
864,847,892,835,749,819,139085,191128,89488,1020,806,804,870,810,804,836,814,843,879,773,831,755,823,814, 2025-03-10 11:48:04.926467
709,727,118154,161163,72882,939,696,659,682,756,716,773,696,712,724,711,713,659,709,701,748,706,670,678, 2025-03-10 11:48:05.124474
852,857,905,856,758,818,139120,191652,89457,1034,823,812,858,835,834,885,830,843,886,790,842,744,819,843, 2025-03-10 11:48:05.322733
719,729,118138,161018,72904,936,711,658,664,761,704,743,690,693,715,700,681,676,691,696,760,709,667,683, 2025-03-10 11:48:05.519547
847,839,877,834,763,801,139485,191888,89571,1056,833,811,845,821,820,913,863,820,893,802,847,739,805,850, 2025-03-10 11:48:05.711350
These are the same histogram data, but normalized for easier reading:
0.002 0.002 0.002 0.002 0.002 0.002 0.318 0.437 0.205 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002
0.002 0.002 0.322 0.439 0.198 0.003 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002
0.002 0.002 0.002 0.002 0.002 0.002 0.318 0.437 0.205 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002
0.002 0.002 0.322 0.439 0.198 0.003 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002
0.002 0.002 0.002 0.002 0.002 0.002 0.318 0.438 0.204 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002
0.002 0.002 0.322 0.439 0.199 0.003 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002
0.002 0.002 0.002 0.002 0.002 0.002 0.318 0.437 0.204 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002 0.002
I'm also indexing a line graph with a zoom on the bins 0 up to 7, normalized and non normalized, as I know reading this histogram data as text can be unbearable.
I've had this behaviour consistent for the whole duration of the test (15 minutes), and I've also observed that the max distance measurement (which is also changing frequently between measurements) has no relation to the histogram data. My understanding is that this histogram should be static as the photons detected are binned according to ToF (which correlates directly to distance).
Am I misinterpreting the data or missing something on the additional data struct? I've not found documentation on the additional data struct nor any other forum posts about this same topic, so I believe this is all expected behaviour and I'm lacking knowlege on the topic. I'm interested in understanding it in the hopes that it helps me solve some other issues I've been solving on this sensor.
I'm using long distance mode, max timing budget (200 ms), no coverglass and no calibrations.
Thanks in advance,
Leonardo